AXIS#.PROFINET.SUPPTELEGRAMID
Description
This parameter is used to select or identify current supplementary data telegram.
If PROFINET.USEMODULECFG = 0, then this command is used to determine which telegram is active.
If PROFINET.USEMODULECFG = 1, then the sub-module/telegram configuration is setup from the PROFINET master and this keyword is blocked.
-
- If setting the value for this keyword, the selected telegram data size must be smaller than the telegram configured in the PLC
"Programmable Logic Controller"
A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines.
Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events for cyclic data to work correctly.
See AXIS#.PROFINET.ACTUALVALUEMAP and AXIS#.PROFINET.SETPOINTMAP
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-04-06-000 |
General Information
| Type | Read/Write |
| Units |
N/A |
| Range | N/A |
| Default Value | 970, 971, 972, 973, 5000 |
| Data Type | Integer |
| Stored in Non Volatile Memory | Yes |
Variants Supported
PROFINET drives: AKD2G-SPP